Selection grid
At any moment you can zoom in or out of the edited diagram (for shortcuts about zooming, see "Using the FFLD Editor").You can also drag the separation lines in vertical and horizontal rulers to freely resize the cells of the grid:

-
-
If a split window is in use, the zoom applies only to the currently selected split window (each split window can be zoomed to different levels).
The current position in the grid is always highlighted by a dotted cell
and its coordinates (row, column) are displayed at the bottom left-hand corner of the editor.
If you click on the current position, then the cell is drawn as gray, meaning that it can be dragged somewhere else in the diagram (see below). You can also select multiple cells with the mouse, or use the arrows of the keyboard with the SHIFT key pressed.
Click on the power rail (gray ruler at the left border) to select a full row.
Other selection commands are available from the keyboard:
| Keystroke | Description |
|---|---|
| Home | moves the caret if pressed again, moves the caret to the head of the network |
| End | moves the caret to the end of the line if pressed again, moves the caret to the end of the network |
| Ctrl + Page Up Down | moves the caret to previous or next network header |
| Ctrl + Home/End twice | moves the caret to the beginning or the end of the program |
| Ctrl + A | selects the whole network if pressed again, selects the whole program |
| Page Up / Down | scroll 1 page |
| Shift-Page Up / Down | selection page up or down |
| Return | equivalent to a double-click |
| Space | change contact or coil |
| Tab | move focus cell right |
| Shift-Tab | move focus cell left |
| Arrows | move focus cell or scroll through ladder |
| Shift-Arrow | multi-select cells |
| Ctrl + F | performs a Search and Replace (+ add hyperlink on the topic) within the whole program |
| Ctrl-Shift-F2 | go to previous bookmark |
| Esc / Shift-Esc | close the rename widget |